cancel
Showing results for 
Search instead for 
Did you mean: 

Pinmap wizard import/export between projects?

aurelien23
Senior
Posted on August 28, 2015 at 16:07

Hello,

In SPC5 Studio V3.4.4, instead of accessing the pinmap wizard using the small icon in the HAL configuration, I created a pinmap wizard in the project using ''New -> SPC5 Studio Pinmap Wizard'' and I'm now stucked because I can't find a way to send this pinmap config to my application HAL config.

There must be a way to do that since creating a pinmap wizard project would have no reason to exist...

Please help! I don't want to reconfigure all my IOs again even if it is ''friendly'' 😉

Thanks for help!
1 REPLY 1
Nickname2551_O
Associate III
Posted on August 31, 2015 at 10:22

Hi Aurélien,

We are looking on a solution to your request

BR

Philippe.