cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F2 USB Host Virtual COM with DMA

rthorstensson
Associate II
Posted on September 01, 2014 at 12:15

I have a module which I need to communicate with virtual com by USB with a STM32F2.

Which means that I need to STM32F2 to be USB host and then connect to the virtual com over USB and I also need the transfer to be done over DMA.

Unfortunatly I cannot find any examples where STM32F2 is USB host for Virtual com. 

Has anyone seen any example code for this or can help me how to achieve this?
2 REPLIES 2
Posted on September 01, 2014 at 16:10

The 2.1 USB Firmware Library has a VCP that works with the STM32F2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
rthorstensson
Associate II
Posted on September 01, 2014 at 18:30

Can you please post  link?

When I google  for 2.1 USB Firmware Library I find:

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32%20Legacy%20Firmware%20Libraries&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD0650...

And on the  OTG examples there is no example where stm32 is USB host for VCP (only when stm32 is device for VCP)