2014-09-01 03:15 AM
I have a module which I need to communicate with virtual com by USB with a STM32F2.
Which means that I need to STM32F2 to be USB host and then connect to the virtual com over USB and I also need the transfer to be done over DMA.Unfortunatly I cannot find any examples where STM32F2 is USB host for Virtual com. Has anyone seen any example code for this or can help me how to achieve this?2014-09-01 07:10 AM
The 2.1 USB Firmware Library has a VCP that works with the STM32F2
2014-09-01 09:30 AM
Can you please post link?
When I google for 2.1 USB Firmware Library I find:https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32%20Legacy%20Firmware%20Libraries&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD0650...And on the OTG examples there is no example where stm32 is USB host for VCP (only when stm32 is device for VCP)