cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F105VC USB_HOST MODE ENUMERATE PROBLEM

halilgeta
Associate
Posted on January 20, 2015 at 12:21

HI,

I try to create a txt file in to a 8gb flash disk (

Toshiba 16GB Hayabusa). I have my own board , dm and dp are direct connected vbus sense pin(pa9) is direct connected to 5V power, there is no any usb connection. I used stm3210c-eval firemware and I define it as FS HOST MODE. The problem is when STM32

can not enumerate device and program go to  HOST_CTRL_XFER.. So always program go to 

HOST_CTRL_XFER after this moment.. 

what stm32 need to enumerate usb flash disk ?

Can anyone help me about this....

0 REPLIES 0