cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_UART_IRQHandler bug?

butenko
Associate
Posted on April 26, 2015 at 21:29

I was struggling for quite a few hours to get the simplest UART input ring buffer working. As soon as an ''overrun'' error occurred, the thing stopped, while the code was prepared to handle that situation (or so I hoped).

After quite a struggle, the following things were observed in the

HAL_UART_IRQHandler

 code:

a) when an Overrun error is detected by the hardware, the huart->ErrorCode field is set

b) if the hardware has received a data byte, the 

UART_Receive_IT

 routine is called;

that routine stores the received byte in the user-provided buffer, decreases the buffer counter, and if it becomes zero (this always happens when we are reading byte-by-byte, using a single-byte buffer), the route calls [user-supplied] 

HAL_UART_RxCpltCallback

Unless the buffer is filled and  

HAL_UART_RxCpltCallback

 is called, the

 UART_Receive_IT

 code does not touch neither huart->Status nor huart->Error fields. 

c) finally, just before completing, 

HAL_UART_IRQHandler

 checks if the huart->Error  field contains some error. If it does, the IRQ routine calls the [user-supplied]

 HAL_UART_ErrorCallback

 routine. But before it does this, it  MODIFIES the State field:

    huart->State = HAL_UART_STATE_READY

Let us review the following situations. For simplicity sake we review only the Receive side of things, ignoring the fact that UART Transfers can take place at the same time:

I) an overrun error is detected, data is received, [remaining] buffer size is 1 byte.

huart->Error is set to Overrrun

UART_Receive_IT

 is called, and moves the input to the buffer: it's the last byte

UART_Receive_IT

 sets huart->State to HAL_UART_STATE_READY, calls

HAL_UART_RxCpltCallback

HAL_UART_RxCpltCallback 

should check for and remember the huart->Error field, and use the new 

HAL_UART_RECEIVE_IT

 call to re-initiate next byte reading.

If the routine itself does not clear the huart->Error field, 

HAL_UART_RECEIVE_IT

 does it in any case;

huart->State is set to HAL_UART_STATE_BUSY_RX

the (c) check in 

HAL_UART_IRQHandler

 is not fired

all is fine and clean for now.

II) an overrun error is detected, data is NOT received

huart->Error is set to Overrrun

UART_Receive_IT

 is not called;

 huart->State

 remains at 

HAL_UART_STATE_BUSY_RX

, hardware is reading data, operation continues

the (c) check in HAL_UART_IRQHandler is FIRED (Error field is not empty):

State is changed to 

HAL_UART_STATE_READY

[user-supplied] 

HAL_UART_ErrorCallback

  is called.

Here we hit the problem:

a)  the user assumes that if their 

HAL_UART_ErrorCallback

  is called, the transaction has been cancelled by HAL. The user tries to start a new one, using  

UART_Receive_IT

 - and it results in an Overrun error appearing again immediately: while the ''software'' part thinks that the hardware is in the idle state, in reality the hardware is still reading data.

b) the user assumes that if their 

HAL_UART_ErrorCallback 

is called, they must record huart->Error code somewhere, but not do anything else, i.e. the operation continues. But now it will never get the next byte: when the byte is received, and the IRQ routine is called, the huart->State field is set to 

HAL_UART_STATE_READY

, and the 

UART_Receive_IT

 will not be called to process the received byte.

III) an overrun error is detected, data is received, but the buffer is longer than 1 byte.

UART_Receive_IT

 is called, and moves the input to the buffer

it's NOT the last byte, 

UART_Receive_IT

  simply returns

the (c) check in 

HAL_UART_IRQHandler

 is FIRED (Error field is not empty):

State is changed to 

HAL_UART_STATE_READY

[user-supplied] 

HAL_UART_ErrorCallback

  is called.

The situation is the same as in case II.

  

Fortunately, in our code we know for sure if there is a reading and/or writing operation pending when our HAL_UART_ErrorCallback routine is called. So, we just restore the huart->Status value back to HAL_UART_STATE_BUSY_RX or AL_UART_STATE_BUSY_TX_RX in that routine, before returning to IRQ.

But this is obviously just a dirty fix, and if the analysis above is correct, it would be nice to have a fix in the HAL_UART_IRQHandler. It looks like huart->State should not be modified there.

#hal #uart
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
henry2
Associate II
Posted on November 30, 2015 at 21:19

(STM32Cube F4 v1.9.0) When using HAL_UART_Receive_IT(), I also encountered the problem you describe.  Upon Rx buffer overrun, the HAL driver does not properly manage its internal states. As you outlined, the driver sets huart->State to HAL_UART_STATE_READY without clearing the Rx interrupt process, resulting in continual Rx interrupts and blocking the application.

I used the dirty workaround you mention:

void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)

{

   if (huart->ErrorCode == HAL_UART_ERROR_ORE) // overrun

   {

      huart->State = HAL_UART_STATE_BUSY_RX;

   }

}

gregkam
Associate II
Posted on December 02, 2015 at 00:05

Hello, On My project I found a similar situation and after many hours/days debugging to find the cause and its solution, essentially I solved with:

 

void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)

{

  //I implement this .. but eventually you can decide with different approach

  //Many macros/proc on this code .. is just to be a hint (mem/rec about this possibility)

  __HAL_UART_CLEAR_OREFLAG(huart);

  __HAL_UART_CLEAR_NEFLAG(huart);

  __HAL_UART_CLEAR_FEFLAG(huart);

  /* Disable the UART Error Interrupt: (Frame error, noise error, overrun error) */

  __HAL_UART_DISABLE_IT(huart, UART_IT_ERR);

 

 //The most important thing when UART framing error occur/any error is restart the RX process 

 if(huart->Instance == USART1)

  {

  

    //Restarting the RX, .. 1 byte. .. u8DATUartShortRxBuffer is My own rx buffer 

    HAL_UART_Receive_IT(huart, u8DATUartShortRxBuffer1, 1);

  }

  if(huart->Instance == USART2)

  {

  

    //Restarting the RX, .. 1 byte. 

    HAL_UART_Receive_IT(huart, u8DATUartShortRxBuffer2, 1);

 

  }

}

===============================================

STM32CubeMX 4.11.0,  Firmware package for Family STM32F0 1.4.0

STM32F042C6Tx uController with LQFP48 package.

UART1Tx = PIN30, UART2Rx=PIN31, UART2Tx=12 and UART2Rx=13

My microcontroller is communicating with another embedded coomunication module (RF/module) by USART2.

Eventually it can help you or somelse too,

Greg

carmine
Associate II
Posted on December 02, 2015 at 14:41

I also confirm the bug, and your workaround solves the issue.

dree86
Associate II
Posted on January 26, 2016 at 08:55

Hi,

I always face noise error (HAL_UART_ERROR_NE) when receive serial data but the solution above works too.

Do you guys know why noise error happend?

Thanks
Jumshed Akhtar
Associate III
Posted on July 12, 2018 at 07:28

I also faced this issue and I fixed by restarting the reception by calling the HAL_UART_Receive_IT() in error callback.  I am receiving one by one byte. I was always calling this API in Rx callback but once this particular corner case occurs of ORE error and no data then UART_EndRxTransfer() is called and UART does not trigger interrupt on reception and hence no Rx call back is called. That's why I called 

HAL_UART_Receive_IT() in error callback for this case.

 Thanks for detailed comment.