cancel
Showing results for 
Search instead for 
Did you mean: 

Is STM32F746G-Discovery working at 100Base Ethernet?

sv1eia
Associate II
Posted on September 17, 2015 at 15:08

Hi,

I would like to know if the STM32F746G-Discovery board can be used as a testbead for 100Base Ethernet.

Christos

1 REPLY 1
Nesrine M_O
Lead II
Posted on September 18, 2015 at 11:42

Hi Christos,

Is STM32F746G-Discovery working at 100Base Ethernet?

Yes.

In fact STM32F746G-DISCO discovery board supports 10M/100M Ethernet communication by a PHY LAN8742A-CZ-TR (U9) from MICROCHIP and integrated RJ45 connector (CN9). Ethernet PHY is connected to STM32F746NGH6 via RMII interface.

-Syrine –