cancel
Showing results for 
Search instead for 
Did you mean: 

TDA7496

meria
Associate
Posted on February 24, 2016 at 09:38

Hi,

Could you please specify the exact pattern of behaving  of TDA7496 at 12V input voltage. When we did a prototype the out put is getting clipped.

Could you please specify the values to get 11V Output wave?

#tda7496
1 REPLY 1
Nickname1623_O
Associate II
Posted on February 24, 2016 at 10:24

Hi Meria ,

you can refer to output power vs supply curve , for 11V power supply input , the output power is around 1W  1% THD @ 4 ohm load , so the unclipping output level is around 2V RMS . for 8 ohm load , it will be around 0.7~0.8W , then the unclipping output level will be around 2.4V RMS .

Thanks to choose ST device.

YT