cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F1 SPI communication with L3GD20 gyro

angelo2399
Associate
Posted on April 21, 2016 at 14:57

Hello everyone!

I currently working on my masters work with STM32F1 MCU. I created work in STM32Cube - SPI2 communication protocol with gyro, UART communication protocol to PC. And everything was fine until I wanna write to gyro (for initialization CTRL_REG1). I try to write on in (i write 0x0F on location 0x20), and then read from same register because I noticed that something was not fine. It returns me every time 0XFF instead of 0x0F.

Gyro: https://www.pololu.com/file/0J563/L3GD20.pdf

I put my code below. Please help me :)

int main(void)

{

uint8_t data_tx = 0;

uint8_t data_rx = 0;

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();

  /* Configure the system clock */

  SystemClock_Config();

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  //MX_I2C2_Init();

  MX_SPI2_Init();

  MX_USART1_UART_Init();

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);

//who am I

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);

data_tx = 0x8F; //we wanna read from address 0x0F

HAL_SPI_TransmitReceive(&hspi2, &data_tx, &data_rx, sizeof(data_tx), 0x1000);

data_tx = 0x00;

HAL_SPI_TransmitReceive(&hspi2, &data_tx, &data_rx, sizeof(data_rx), 0x1000);

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);

HAL_Delay(500);

//initialization CTRL_REG1 (20h)

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);

data_tx = 0x20; //register address 

HAL_SPI_TransmitReceive(&hspi2, &data_tx, &data_rx, sizeof(data_tx), 0x1000);

data_tx = 0x1F; //mode 

HAL_SPI_TransmitReceive(&hspi2, &data_tx, &data_rx, sizeof(data_tx), 0x1000);

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);

HAL_Delay(500);

//read from CTRL_REG1 (20h)

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);

data_tx = 0xA0; //register address 

HAL_SPI_TransmitReceive(&hspi2, &data_tx, &data_rx, sizeof(data_tx), 0x1000);

data_tx = 0x00; //mode 

HAL_SPI_TransmitReceive(&hspi2, &data_tx, &data_rx, sizeof(data_tx), 0x1000);

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);

HAL_Delay(500);

  while (1)

  {

HAL_UART_Transmit(&huart1, &data_rx, sizeof(data_rx), 0x1000);

HAL_Delay(1000);

  }

}

/** System Clock Configuration

*/

void SystemClock_Config(void)

{

  RCC_OscInitTypeDef RCC_OscInitStruct;

  RCC_ClkInitTypeDef RCC_ClkInitStruct;

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.HSICalibrationValue = 16;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

  HAL_RCC_OscConfig(&RCC_OscInitStruct);

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);

  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);

  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

  /* SysTick_IRQn interrupt configuration */

  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

}

/* SPI2 init function */

void MX_SPI2_Init(void)

{

  hspi2.Instance = SPI2;

  hspi2.Init.Mode = SPI_MODE_MASTER;

  hspi2.Init.Direction = SPI_DIRECTION_2LINES;

  hspi2.Init.DataSize = SPI_DATASIZE_8BIT;

  hspi2.Init.CLKPolarity = SPI_POLARITY_HIGH;

  hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;

  hspi2.Init.NSS = SPI_NSS_SOFT;

  hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;

  hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;

  hspi2.Init.TIMode = SPI_TIMODE_DISABLE;

  hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

  hspi2.Init.CRCPolynomial = 10;

  HAL_SPI_Init(&hspi2);

}

/* USART1 init function */

void MX_USART1_UART_Init(void)

{

  huart1.Instance = USART1;

  huart1.Init.BaudRate = 115200;

  huart1.Init.WordLength = UART_WORDLENGTH_8B;

  huart1.Init.StopBits = UART_STOPBITS_1;

  huart1.Init.Parity = UART_PARITY_NONE;

  huart1.Init.Mode = UART_MODE_TX_RX;

  huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;

  huart1.Init.OverSampling = UART_OVERSAMPLING_16;

  HAL_UART_Init(&huart1);

}

/** Configure pins as 

        * Analog 

        * Input 

        * Output

        * EVENT_OUT

        * EXTI

*/

void MX_GPIO_Init(void)

{

  /* GPIO Ports Clock Enable */

  __HAL_RCC_GPIOB_CLK_ENABLE();

  __HAL_RCC_GPIOD_CLK_ENABLE();

}

0 REPLIES 0