cancel
Showing results for 
Search instead for 
Did you mean: 

um0233 library with STR912FW44

robosoft
Associate II
Posted on February 13, 2008 at 06:17

um0233 library with STR912FW44

6 REPLIES 6
robosoft
Associate II
Posted on May 17, 2011 at 09:49

Hi,

To solve the spurious interrupt problems, i use the new library (um0233).

My application, its works with an older library, does not work.

So I have written a very small program that toggles P6.0.

 

int main(void)

 

{

 

 

GPIO_InitTypeDef GPIO_InitStructure;

 

 

//INIT SCU

 

SCU_PLLFactorsConfig(192,24,2);

 

SCU_PLLCmd(ENABLE);

 

SCU_PCLKDivisorConfig(SCU_PCLK_Div1);

 

SCU_HCLKDivisorConfig(SCU_HCLK_Div1);

 

SCU_FMICLKDivisorConfig(SCU_FMICLK_Div1);

 

SCU_BRCLKDivisorConfig(SCU_BRCLK_Div1);

 

SCU_APBPeriphClockConfig(__GPIO6 , ENABLE);

 

 

//INIT GPIO6

 

 

GPIO_DeInit(GPIO6);

 

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

 

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

 

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

 

GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable;

 

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt1;

 

GPIO_Init (GPIO6, &GPIO_InitStructure);

 

 

//SQUARE WAVE

 

 

while (1)

 

{

 

GPIO_WriteBit(GPIO6,GPIO_Pin_0,Bit_SET);

 

GPIO_WriteBit(GPIO6,GPIO_Pin_0,Bit_RESET);

 

 

}

 

}

 

I link the 2 startupfiles included with the library.

With the old library I get a square wave, with the new lib nothing appears on the output.

I use Keil RV ARM with a STR912FW44 device on custom hardware.

Is this libary (for FA devices) compatible with FW devices ?

Thanks

Luc Vercruysse

amira1
Associate II
Posted on May 17, 2011 at 09:49

Hello robosoft.ontwikkeling,

Normally, the new library version is validated on the rev FA silicon. Please refer to the application note: migration from STR91xF to STR91xFA. There are some new features supported by some IP like the ADC (external pin trigger feature for example) which are recovered by our library examples.

However, there are no enhancement in the GPIO.

Best regards,

mirou.

robosoft
Associate II
Posted on May 17, 2011 at 09:49

Hi,

When I use the original startup code from KEIL in above testprogram, the GPIO works fine. It seems that the part that inits the FMI causes the problem with the GPIO !??? However, this is not the solution for other problems I have (CAN bus is not working, function that returns the clockfrequency gives a result 24MHz i.s.o. 96MHz ect...) With the old library and startupcode i did not have that kind of problems (except interrupt ..) I wonder if KEIL startup code can be modified to have the same work around for the interrupt problems ? I am not very familiar with assembler .

I have ordered a FA device from RSComponents, so I I can try it with the new device tomorrow ! I hope I have some positive results !

The STR912 replaces a 80188EB witch is end of life. Quiet some software has been rewritten already, hardware has been redesigned ...Deadlines reaching the end as our stock of 80188EB decreases ...

Regards

Luc Vercruysse

robosoft
Associate II
Posted on May 17, 2011 at 09:49

Hello,

It is a full version.

IDE-Version:

µVision3 V3.55a

Copyright (c) Keil Elektronik GmbH / Keil Software, Inc. 1995 - 2007

Tool Version Numbers:

Toolchain: RealView MDK-ARM Version: 3.15b

Toolchain Path: BIN31

C Compiler: Armcc.Exe V3.1.0.914

Assembler: Armasm.Exe V3.1.0.914

Linker/Locator: ArmLink.Exe V3.1.0.914

Librarian: ArmAr.Exe V3.1.0.914

Hex Converter: FromElf.Exe V3.1.0.914

CPU DLL: SARM.DLL V3.15b

Dialog DLL: DARMST9.DLL V1.03

Target DLL: BIN\UL2ARM.DLL V1.32

Dialog DLL: TARMST9.DLL V1.01a

Kind regards

Luc Vercruysse

jilisegiar
Associate II
Posted on May 17, 2011 at 09:49

which version are you using and is it trial or full version?

truf9
Associate II
Posted on May 17, 2011 at 09:49

Hello,

I have the same Keil-Version and have included the STR91x library V2.0 in my project.

In the project I use STR91x.S as Startup-File.

I use the GPIO6 Pin3-6 for leds. This works also with the new STR91x library V2.0.

Here's a copy from parts of my source:

SCU_MCLKSourceConfig(2);

SCU_PCLKDivisorConfig(SCU_PCLK_Div8);

SCU_PLLFactorsConfig(128,25,2);

SCU_PLLCmd(ENABLE);

SCU_MCLKSourceConfig(0);

SCU_APBPeriphClockConfig(__GPIO6, ENABLE);

// Test this ->

SCU_APBPeriphReset(__GPIO6, DISABLE);

My project works with CAN-Bus (1M), 2xSPI-Bus, 2xUART and GPIO's

What are the frequecies shown in Power,System and Clock Control unit in the peripherals of uVision.

If I load your PLL-Faktors the CPU-Clk is at 100MHz.

Best Regards