cancel
Showing results for 
Search instead for 
Did you mean: 

Sharing Revolutionary and Free embedded development tools for ARM Cortex

ahnniu
Associate II
Posted on October 11, 2009 at 16:34

{Sharing} Revolutionary and Free embedded development tools for ARM Cortex

2 REPLIES 2
ahnniu
Associate II
Posted on May 17, 2011 at 13:25

Dear All,

1. Do you still around to look for Free embedded development tools?

2. Do you still spend a lot of time to prepare for driver? Or struggling to learn the driver programer the official provided?

3. Do you still spend a lot of time to transplant RTOS or TCP/IP, USB protocol stack?

4. How much time is actually used in the development of the business logic?

Reality:

You spend too much time in the preparation of some of the key, but not the core part. The time you have left to the application development is too little.

Revolutionary things:

1. Have you ever tried to directly check to select the driver, RTOS, TCP/IP protocol stack through the mouse, without having to care about migration issues, and to easily view the help and examples?

2. Have you ever tried to generates an driver example through a mouse click?

3. Have you ever tried to simply generate a set of solutions by mouse, then compile, download and run in the target board?

http://www.coocox.org/CooCox_Builder.htm

Only For ARM Cortex M3, STM32 Series for example, has equipped with these features. So you can fully concentrate on the development of application software.

You can visit

http://www.coocox.org/CooCox_Builder.htm

to get more information.

CooCox Builder V0.1 can only build and has not been tested completely, it only for the users who always give attention to us.

----------------------------

http://www.coocox.org

, Cooperate on Cortex, Free and Open RTOS, Free embeded development tools For ARM Cortex M3.

tomas23
Associate II
Posted on May 17, 2011 at 13:25

The ActiveX thingy for download is quite unhappy solution... Anybody tested it already?