cancel
Showing results for 
Search instead for 
Did you mean: 

USART full duplex

greg_t
Associate II
Posted on September 29, 2010 at 22:26

USART full duplex

1 REPLY 1
Posted on May 17, 2011 at 14:09

Well there is ''one'' register in terms of the address presented for you to read and write, but in terms of the hardware you are writing to a TX buffer register (which is moved to the TX shift register when the last bit shifts out), and reading from a different RX buffer register (which is loaded from the RX shift register when the last bit has shifted in).

They are independent, but share the same IO address. The USARTs are full duplex.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..