cancel
Showing results for 
Search instead for 
Did you mean: 

SPI connect to SPWF01SC

christos
Associate II
Posted on July 02, 2015 at 16:04

Hi,

I'd like to use the SPI connection of SPWF01SC.

Could you say me please which pinout description are right?

Is the the DocID025635 Rev 2 and the STEVAL-IDW001V1 with SPI description right?

http://www.mikrocontroller.net/attachment/229286/spwf01.pdf

Or the DocID025531 Rev 5 without SPI?

http://www.st.com/web/catalog/sense_power/FM2185/SC1930/PF258592

Thanks
3 REPLIES 3
Posted on July 02, 2015 at 16:10

Hi Chris,

there is no SPI interface on SPWF module

Posted on July 02, 2015 at 16:32

SPI, I2C, etc, are peripherals from internal STM32.

They are exported on module's GPIOs, but cannot be used with a standard firmware.

Standart FW only allows AT-commands through UART. I'm sorry for misunderstanding.