cancel
Showing results for 
Search instead for 
Did you mean: 

Importing SPC5Studio V3.5 project using V5.0

dinesh
Associate
Posted on October 27, 2016 at 14:46

Hi,

I need to work on old project created using SPC5Studio V3.5. Project is created using Wizards. When I open same project using V5.0, the 'Configuration.xml' is showing some error (red cross against file name). If I try to generate new code using 'Configuration.xml' it is giving following error messages

hal_lld.h 1.0.0.201609071703 : ...CAN NOT APPLY THE PATCH...

FlashMap.h 1.0.0.201609061636 : ...CAN NOT APPLY THE PATCH...

Am I doing something wrong?

First time I am using SPC5Studio

1 REPLY 1
procolo
Senior
Posted on November 07, 2016 at 10:34

Hi,

there should be a problem importing old project into new 5.0. some files massively changed , so it could be a prolem patching new files with old patch.

My suggestion is to create a brand new project in 5.0 and then reapply the patches on those files.

Regards