Skip to main content
waclawek.jan
Super User
December 21, 2017
Question

['F446 documentation] What is CKGATENR in RCC?

Posted on December 21, 2017 at 23:15

.

This topic has been closed for replies.

2 replies

ST Technical Moderator
December 26, 2017
Posted on December 26, 2017 at 17:20

Hello

Waclawek.Jan

,

The CKGATENR register allows to enable the clock in continues to these peripherals even if they are not used.

Kind Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Jan Waclawek
Visitor II
December 28, 2017
Posted on December 28, 2017 at 14:16

Hi Imen,

Thank you for the answer. However, it rises even more questions.

The CKGATENR register allows to enable the clock in continues to these peripherals

even if they are not used.

I struggle to understand the 'not used' part.

The peripherals in question are

1. the two AHB-to-APB bridges,

2. debug module in processor

3. SRAM (there is a typo in the description, 'SRQAM')

4. FLITF (the internal FLASH interface)

5. RCC

There is a 'SPARE' bit which I assume is erm... just a spare... Correct?

Now I can see that the debug module can be unused if there's no debugger attached. I could imagine the bridges to be unused if all attached peripherals on given APB are switched off - but I doubtt this is the case. And I cannot see any scenario under which could SRAM and RCC be unused.

So, can you please elaborate, what 'unused' in this context means, what are the ramifications of said clock gating and what is the reason for having it disabled through this register?

Thanks,

Jan Waclawek