cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK/V2 with Low Power mode

Stefan Hittinger
Associate II
Posted on June 27, 2017 at 16:06

With our custom board (STM32F103) i debug with Segger J-Link. No Problem with 'WFI' instruction.

Now i tried to use ST-LINK/V2 with latest firmware (2-28). Download and single step actions are ok, but in run mode the application stops at 'WFI' and nothing more happens. When i halt the debugger the program counter is located after the 'WFI'. With single step i can walk through my code. All goes correct.

It seems that all interrupts are blocked until i stop the debugger.

Is ST-LINK/V2 not able to work with Low Power modes?

0 REPLIES 0