cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F051x programming system memory

Daniel Manso
Associate
Posted on June 27, 2017 at 10:02

hi everyone,

i�m working with the STM32F051.

I want to programm the System memory over the Serial interface using the ST Flash Loader Demonstrater.

So i set the BOOT0 Pin high, and connected the STM32F051 to the Computer.

Now i tried to use the ST Loader Demonstrater and i got the error message:

'This Version is not intended to suport the <STM32F0_63K> target'.

The communication is possible when i�m using a terminal Programm and the Commands from the 'AN3155'.

Now my question:

is there any other way to programm the STM32F051 System Memory without sending single commands over an terminal programm?

Hope i made the problem clear.

I allready thank you for your help.

#programming #stm32f051x #system-memory
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Zt Liu
Senior III
Posted on June 27, 2017 at 10:21

hi,

You want to PROGRAM the system memory?

or

You want to run the boot-loader from system memory and program the FLASH memory?

Is the former possible?

Daniel Manso
Associate
Posted on June 27, 2017 at 10:33

of course the second one

misagh
Associate III
Posted on June 27, 2017 at 11:22

A little easier way for programming your flash memory is to make a batch file with your commands. Therefore, it is not need to write the command every time you want to program the flash memory.

Bests,

Misagh