Hello, Likely drawing signals will help to better understand your needs. Do you need that the sixth timer starts in free-running mode, without waiting for the same SYNC as others?You can configure the External Event Signal as a reset source for the s...
Hello Benedikt, What may be missing in the information you gave above is the system clock frequency to programmed. The DAC underrun may be caused by the priority conflict between cpu access to hrtim (requiring code execution and ram access) and then ...
Hello, I understand that you want to apply to deadtime on both edges of Timer E output (active low). Functions below are not applied on the same Timer Unit? is it what you intend?LL_HRTIM_DT_SetRisingValue(HRTIM1, LL_HRTIM_TIMER_F, value_to_set_hv);L...
Hello, In case you are using the HRTIM, you can use the mode Single-shot.In this mode the counter is started by a reset event and it stops when it reaches the period value set in the HRTIM_PERxR register.The reset signal would be the input signal con...
During the start-up phase, the reference value is updated smoothly (using the systick routine) to reach the final reference value incrementally. I suggest that you generate the compensation coefficients based on the highest output voltage and use thi...