User Activity

Hello!Is there any additional information about on how to use on ST25R3916 the bypass mode of internal VDD_RF regulator to be able to a transmitter output current higher than 350 mA (up to 500 mA) supplied from an external source.In ST25R3916 datashe...
Hello!Can you tell me the reasons and meaning of the necessity of grounding the center of the ST25R3916 antenna loop?In X-NUCLEO-NFC08A1 the jumper between the center of the antenna loop and ground is closed, but in ST25R3916 Discovery Board it is op...