User Activity

Hello.When I measure between 5V_SCR1 and GND_SCR2 in STEVAL-DPSTPFC1 Hardware, I see 9V. And when I start via Switch, it goes into standby mode when the output is unloaded and reaches 300V. It never becomes 400V. I quickly turn the switch to the off ...
hello,I have STEVAL-DPS334C1 and STEVAL-DPSTPFC1. I am trying to put PFC code on STEVAL-DPS334C1 again. I load bin file via stm32programmer. then STEVAL-DPS334C1 crashes. I need source code to find where the error is coming from. Or if you have any s...