cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-DPSTPFC1 Hardware Problem

BerkMaviengin
Associate

Hello.When I measure between 5V_SCR1 and GND_SCR2 in STEVAL-DPSTPFC1 Hardware, I see 9V. And when I start via Switch, it goes into standby mode when the output is unloaded and reaches 300V. It never becomes 400V. I quickly turn the switch to the off position again. I quickly turn it back to the on position. This time, all the LEDs go off. Can you please tell the technical team where the error and problem may be?

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @BerkMaviengin, to the community!

Is there a special reason why you measure between 5V_SCR1 and GND_SCR2, which have nothing to do with each other? GND_SCR1 belongs to 5V_SCR1?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.