User Activity

It's very hard to add it without instructions to not break existing infrastructure with LoRa.When I run simple example generated from classic .IOC file I got the I2C running without a problem.The board I'm using: Murata Type 1SJ
The reason I'm looking for it is because I was able to run SubGHz_Phy successfully but I'm unable to enable the I2C or GPIOs at all. The board I'm using: Murata Type 1SJBest Regards.Milan
I need ST Motor Control Workbench v5.4.1. because my motor won't start after project generating with v5.4.3.
Posted on February 25, 2016 at 11:27Hello,I need advice about AES 128 or AES 256 implementation in STM32L0 series. What is the best solution? Do I have to use the controller with AES hardware accelerator or there is a software solution that is fast ...
Posted on November 06, 2015 at 19:48Interrupt is working good when STM is in run mode, but when STM enter STOP mode interrupt from pin PC12 doesn't work, end after that interrupt doesn't work at all, even when STM enter run mode againt. It's seems l...