User Activity

I am using a STM32F103 and having issues to make an USB application.I generated the project using CubeMX and I am not being able to transmitt a message.Here is the configuration:Main is like this (It is C++ in case it matters): int main(void) { H...
I am trying to use stm32F446 as a master I2C device with LL library and I have 2 main issues.1. After sending a couple of messages(always 4 at most) over I2C I get no start condition when setting CR1->START, if I pause the program a couple of seconds...
I am using LL library on STM32F446 for an I2C master, I am trying to comunicate with a device with 0x7B address, after sending the address I don't get the ADDR flag, insted I get ADDR10Here is my interrupt code: if (LL_I2C_IsActiveFlag_SB(I2C1)) {...
I am trying to comunicate a stm32F103C8T6 with an STM32F446 over I2CFirst thing I try to do is send data as master from F103 and I get NACK by F446Here is logic analyzer's screenshot:And here is F446 configuration on CubeMXI don't get why is it sendi...
I am planing to have a time functionality on a project I want to make.After reading the manual I undestood I have a 32 bit counter which increases with TR_CLK.Let's say I want to update the clock every 1ms, that would leave me with aproximately 49.5 ...