[Solved]I needed to modify the option byte using the STM32Prog. Once changing the Option Byte BOOT_SEL to 1, and Then BOOT0 and BOOT1 to 1. It now works.
Hello, I am getting the same complication with my device. Its a STM32L010K4Tx. Which has no boot pin. I am using an ST-Link v3 mini which works are programming and unbricking the device. When the device is operating standalone, it isnt operating its ...