User Activity

Hello,I can't use SMR library in GNU toolchain as only hard fp version is available from ST. I can't use hard flag to compile my application as I have other libraries compiled with soft.Thanks and Regards,Dario
We have a IMP34DT05 interfaced with a STM32L486 on PDM. We are observing that, after the clock to the MEMS is enabled and the sampling is started, in the first 10 seconds unexpected db values are calculated (higher than expected: 80 db). Then, the v...
I've CUBE-MX 5.3.0 ant I'd like to add package  X-CUBE-MEMSMIC1.It's not in the list of embedded packages shown in CubeMX.I've downloaded tha .zip from:https://www.st.com/en/embedded-software/x-cube-memsmic1.htmland I tride to install it "from local"...
I use dual flash bank in STM32L4. I perform a flash bank switch by programming bit BFB2 in OPTR.Sometimes, after the new software has started, RTC seems to be returned to reset state: date and time are lost and RTC internal registers are cleared! In...
Posted on January 15, 2018 at 10:36Hello,Rx signal from an external card is forked (by HW) to the pins of STM32L486RGT6:- UART5 RX (PD2);- PC13 (Wakeup#2).Then, a reception from UART 5 will wake up the microcontroller from Standby mode (this is OK)....
Kudos from