User Activity

I'm trying to use a RS422 transceiver set up between ST Motor Pilot and EVSPIN32G4 development board.I'm using an FTDI USB-Serial converter and two RS422 Transceivers with /RE and DE signals.Is it possible using the ST Motor Pilot to use these hardwa...
I am having false Over Current conditions when the inverter board starts up, before any kind of operation.Motor Pilot shows Over Current fault that happened but FAULT_OVER, most likely a short condition that prevents further operation without acknowl...
Trying to update a test project from MC Workbench, I get the error "Fail to copy Extra folders" and generation fails.Log shows:2024-11-19 12:40:56,300 ERROR [Wb2MxProcess.copyExtraFolders] Fail to copy Extra foldersThese are the steps to reproduce:- ...
Hi,I am developing on EVSPIN32G4, MC Workbench 6.1.2.The only option for Over Voltage Protection is to turn on Low Side Switches. This unfortunately doesn't work as I still constantly get Over Voltage faults in position control mode, when the motor i...
Hello,I started development on the EVSPIN32G4 development board. After generating the project in MC Workbench, the resulting CubeMX project shows up with a STM32G431VBTx MCU. This is a LQFP100 package, but the STSPIN32G4 is only a 64pin device. I am ...
Kudos from