Skip to main content
Associate II
December 2, 2024
Question

Motor Pilot and FTDI RS422/485 - Is it possible?

  • December 2, 2024
  • 0 replies
  • 455 views

I'm trying to use a RS422 transceiver set up between ST Motor Pilot and EVSPIN32G4 development board.
I'm using an FTDI USB-Serial converter and two RS422 Transceivers with /RE and DE signals.

Is it possible using the ST Motor Pilot to use these hardware flow control signals to set the transceivers in RX/TX modes as transmission occurs?

This topic has been closed for replies.