User Activity

Posted on April 27, 2016 at 15:43Hi all,I'm just starting to embark on the problem of accessing external registers (implemented in a FPGA), via the FSMC on the STM32F4 core.  What I'm interested in doing is accessing these registers as SRAM (memory ...
Posted on February 07, 2016 at 09:12Hi all,I have an issue with SPI on the STM32F401VC microcontroller.  What seems to be the problem is that the SPI device (SPI1) doesn't seem to drive the completion flags correctly on the hardware.  For example, I...
Posted on September 10, 2015 at 16:57Hi all,I've just started playing with the STM32F4 on the STM32F401C Discovery board, and had some strange behaviour (slowed down time) when attempting to generate a 1ms TIM2 interrupt.From the reference manual fo...
Posted on September 10, 2015 at 15:28Hi all,I've just started playing with the STM32F4 on the STM32F401C Discovery board, and had some strange behaviour (slowed down time) when attempting to generate a 1ms TIM2 interrupt.From the reference manual fo...
Posted on September 10, 2015 at 13:30Hi all,I've just started playing with the STM32F4 on the STM32F401C Discovery board, and had some strange behaviour (slowed down time) when attempting to generate a 1ms TIM2 interrupt.From the reference manual fo...