Thank you for your question.1) The difference between L9369 and L9370 is whether it's VDA 3.0 compliant or not.2) The gate driver block is the same for the L9369 and L9370.3) Need to check if L9370 datasheet is available on the open market. Please co...
Thank you for your question.Output levels are programmed through SPI_GIOx_HSCtrl (reg 0x77) and SPI_off_GIOx (0x87) bit, the following table shows the behavior of the system according to the configuration bits:Thanks.