User Activity

Problem:I'm working with an STM32H743 and trying to generate a PWM signal (Center Aligned) on PE9 using Timer1 (TIM1). Although the PWM output is functioning, the frequency is not what I expect. I’m trying to generate a 1 kHz signal, but instead, I’m...
I’m working with an encoder that has a specification of 1024 pulses per revolution (p/r), and it will operate at a maximum speed of 1500 RPM. At this speed, the signal frequency produced by the encoder is approximately 25.6 kHz.The encoder outputs a ...
Kudos given to