update:code and .ld file is generated correctly with 6.12.0 but not with 6.12.1 (for a makefile project)Tested with the existing project* and a new one. does not seem to relate to the firmware package version, even with 'STM32Cube FW_L4 V1.18.1' it w...
Well, just updated CubeMX (Windows) and ran into the same issue. diff between STM32L432KCUx_FLASH.ld (generated after update, faulty)and ACP14_STM32L432KCUx_FLASH.ld (the previous version of that file, working)10c10
< ** 256Kbytes FLAS...