User Activity

 Hello I'm developing RTOS environment of dual-core in STM32H757.Using the functions osThreadResume and osThreadSuspend now I'm programming the context swtiching.Recently, I found  a good approach : context switching using the functions osEventFlagWa...
 Hello I'm developing RTOS environment of dual-core in STM32H757.I could refer to the examples provided by STM32, and I read the application note AN5617. I checked that the error is a exception "err1" under the function "rproc_virtio_create_vdev" in ...
Hello I'm developing RTOS environment of dual-core in STM32H757.I could refer to the examples provided by STM32, and I read the application note AN5617. I want to set OPENAMP_M4 Communication Mode to Master, so I would like to find a project with OPE...
Hello I'm developing RTOS environment of dual-core in STM32H757.In OpenAMP communication mode, CM4 is the master and CM7 is the slave, and I used SRAM4 to create SHMEM.I could refer to the examples provided by STM32, and I read the application note A...
Hello Error Definition1 : the return value of the OPENAMP_send function is 4. // RPMSG_ERR_NO_MEM?Error Definition2 : the return value of the OPENAMP_send function is -2007. // RPMSG_ERR_ADDR I'm developing RTOS environment of dual-core in STM32H757....
Kudos from
Kudos given to