User Activity

Hello there,I'm using stm32h747i-DISCO board, and running object detection demo from model-zoo. Now i want to add Ethernet functionality with the demo. I have some questions for the same, as below...Q1) there is only one linker script in object detec...
Hello there,Using stm32h747i disco board: azureRTOS + netxduoI have added azure RTOS and netXDuo on CM4, I want to run MQTT on Ethernet. I have done below changes on the board.I have connected the LAN cable from board to laptop for peer to peer conne...
Hello there,I have STM32H747I-DISCO and ov5640. Can i use ov5640 for model-zoo ? If yes what changes are required ? I'm following repo : https://github.com/STMicroelectronics/stm32ai-modelzoo/tree/mainI have already installed the "requirement.txt"How...
Kudos given to