User Activity

Hello.I am trying to migrate from stm32f407vgt6 to stm32h742vgt6, is there any difference in spi specifications?Please give me your best regards.
When I try to write to stm32h742vgt6 using stlink-v3minie, Target is not responding, retrying... and cannot write.The same microcontroller can be written to the board on which it is mounted. In the same program.What are the possible outcomes in this ...
I want to use arm_math.h in stm32cubeide. Best regards.
Hello.I tried to use an imu that was previously working using the spi2 port of the stm32f4 series with the spi4 port of the stm32h7 series, but I cannot communicate with it. (imu is using icm42688p.)Is it possible that I have made a mistake in my set...
Hi guys,I am currently trying to read the value of the WhoAmI register using SPI communication with the ICM42688P, but it returns 0xf3 when it should return 0x47. Is there something wrong with my program or configuration?Please tell me about it. .hpp...
Kudos from
Kudos given to