Posted on June 22, 2015 at 23:36I have a F4 chip that calls , The function initiates a system reset request to reset the MCU.__STATIC_INLINE void NVIC_SystemReset(void) { __DSB(); /* Ensure ...
Okay, there is two days of my life gone on this bug. Thanks for defaulting all the pins to NO-PROGRAMMING/DEBUG.After checking all the hardware connections.The st-link still could not connect to the device (no communications).Figured that some where ...
Posted on June 23, 2015 at 21:28Thanks for the fast reply Clive, We couldn't fault the hardware, BootPins etc or the code, so we lifted the chip. And it is all good. Don't know why it missed behaved. ESD maybe but the usual precautions are in ...