cancel
Showing results for 
Search instead for 
Did you mean: 

FATFS library R0.15 not available on ioc configurator

danirpg
Associate II

Hi,

Im starting a new application on a custom board with a STM32H753ZIT, i see when added the FATFS lib from middleware the version of elmchan version is the R0.12c but i see also in the git of the stm32 STM32 FATFS GIT a release of the R0.15 but in the configurator i cant select the R0.15.

 

There will be soon any update on the stm32cube sw to show this version of the fatfs in the short time?

1 REPLY 1
Andrew Neil
Super User

https://community.st.com/t5/stm32cubemx-mcus/nucleo-c031c6-board-and-sd-card-interface-by-spi/m-p/728814/highlight/true#M29770

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.