User Activity

Hi,I am trying to read device id of the W25Q16JV Flash Memory (3V 16M-BIT SERIAL FLASH MEMORY WITH DUAL/QUAD SPI) using the STM32G474RBT4 Nucleo board via QSPI lines.I hereby attach the ioc settings and the code used:static void MX_QUADSPI1_Init(void...
Hi, I am using STM32L412RB MCU and I need to configure STuW81300 - EVB using SPI. I need an example code for reference. Suggest any relevant examples or programming manuals. Any example of this same or any SPI implementation of STuW81300 would be ver...
I need to read/write data into the external Serial NOR Flash (MX25U25645GMI00) via Quad SPI of STM32L412RB board using STM32CubeIDE.I was able to get the Device ID of the MX25U25645GMI00.I am unable to write/read data into the MX25U25645GMI0 in Auto ...
Kudos from