User Activity

Hello everyone,I need to implement the burst controller in HRTIM in order to load 3 compares of the master timer at once.I am using low layer so I do not have a lot of info.My .ioc setting are:Then, in the DMA CH1 interruption I have something like t...
Hello everyone,I am generating PWM signals using the HRTIM module. Specifically, I am using Timer D to generate a PWM signal along with its complementary signal. This signal is always in phase with the master counter, setting at the timer period and ...
Hi all!I have NUCLEO stm32G474RE board, and I am playing with HRTIM.I am trying to take advantage of fault logic, found in HRTIM module.HRTIM can have GPIO hardware input, which can shut down all HRTIM outputs, without any software overhead.Now, I wo...
Dear team,I am using a STM32G474 in my application. I've generated a PWM in the HRTIM TIMER E that is active low (necessary for the requirements of the modulation). I want to insert a dead band between this signal and its complementary (Output 2). Th...
Kudos from
Kudos given to