User Activity

Well, I'm developing a system for reading sensors and sending them to a server.I'm using a GSM LTE module to do this sending. At first it worked well, but after a while the system stopped sending messages to the server.We can see this clearly in the ...
I'm developing a system with a GMS module, where AT commands are sent to the module via an STM32L0.In this case, I'm having problems with the AT+CSTT command, which was giving me an ERROR. After a lot of thought, I realized that the error was due to ...
I'm developing a vibration and temperature analysis system.To do this, I have developed a sensor based on an STM32L053C8 chip and a KX122-1037 accelerometer.Looking at the datasheet, this accelerometer can reach a maximum data rate of 25600Hz, which ...
I'm developing a vibration and temperature sensor solution for industrial machinery.Previously, my system was equipped with Atmega 328p chips, but it has now been upgraded to an STM32LO53C8T8 chip.The circuit has a LoRa radio for sending signals to t...
I have a system of sensors connected to an STM32 chip, all working via I2C and 3.3V.I've created interface libraries for my sensors, specifically the temperature and accelerometer ones. However, when I read the values measured by the sensors, I came ...
Kudos given to