2015-10-06 11:31 PM
hi ! there is a hard to knowing about scand mode with ADC for me
i using hal library set up it by CubeMX there is real code send at link below so - at line 142 delare attribule withMX_ADC_Init() function
- i start ADC sampling process at line 81 - and in forever loop i pooling the ADC convertion and expect the led in pin 10 will be on if the vol signal in PIN ADC CHANNEL over 3v so the led has been on when i just touch the fingure on itand is it each of channal ADC in the regular group will be convert in while loop ????
please help me about it thank so much
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.