User Activity

Hello everyone, I want to measure the current consumption in low power modes on a STM32WB5MMDK discovery board, I would have two questions  1) I have clock issues when I want to use MSI clock to have a 2MHz SysClk to put my STM32 board in Low run pow...
Hello everyone, I want to measure the current consumption on a STM32WB5MMDK discovery board. I've found that I had to put an ammetre on the jumper JP1, and I programmed the RGB LED to be working. However, when I put the ammetre and I power my board, ...
Good afternoon, I am currently working with the STM32WB5MMDK. Upon verifying the documentations, I couldn't find any mention of a JTAG interface for debugging purposes. I wanted to know if the JTAG pins can be used for programming and debugging as SW...
Hello everyone,I am working with a STM32WB5MMDK. I want to use the USART to print a message on Tera Term but i just have inversed triangles instead of "Hello world". I checked and both Tera Term and USART1 have the same parameters (baud rate, etc). I...
Hello everyone,I am working on a STM32WB5MMDK. I already posted a question about the BSP example.I have few other questions about it.I wanted to replace the Button 1 by the Button 2 so I changed it in the main file (even the CallBack). I checked the ...
Kudos from