User Activity

HI Forum,I am configuring my USART as a synchronous slave receive only, the cube software configures clock, receive and transmit GPIO and I cannot remove the transmit GPIO configuration in the GUI without it removing the entire peripheral.  Is their ...
I am using an STM32F769NI with a MT48H16M32LFB5-6 SDRAM chip, everything works fine. we are looking to set the drive strength to 1/4, 1/2 and full to evaluate the effect on EMC testing. From what I read in the programming manual, it states to perform...
I am using an STM32F769NI with a MT48H16M32LFB5-6 SDRAM chip, everything works fine. we are looking to set the drive strength to 1/4, 1/2 and full to evaluate the effect on EMC testing. From what I read in the programming manual, it states to perform...
For a little background, i have modified the project to take audio data from a static file to eliminate any issues with interrupts from the mems microphones may have been causing though the result is the same. I have also added print statements to t...
Posted on July 12, 2016 at 08:23Hi everyone, I have a display hooked up to an STM32F767 via the FMC and all is working properly.  When I try to use DMA2D the DMA2D will only transfer the first 64K of data.  There is no error generated, it appears to...