User Activity

Hello,I have successfully implemented a Touchgfx based UI app using cubeMX and freertos on the STM32U599 chip. This is a basic application with multiple screens, a number of components all in ARGB2222. I am now in the process of porting my app from F...
Hello, I am facing an issue where the rendered frame buffer is printed on the display as gibberish pixels.I'm using the Nucleo F746ZG and interfacing it (over SPI) with an external display controller that writes to a 240*320 display. I was not able t...
Hello, I am working on a TouchGFX (4.23.2 release) project with the Nucleo-F746ZG. I was able set up my registers in cube mx and use the designer to generate for for screens and custom widgets. However, I get a when any of the Matrix3x3 methods are c...
Kudos given to