cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with RF Distance Range between 2 Nucleo-WL55JC2 ?

joe_lambord
Associate II

Hello, I am testing two STM32WL55. I have two NUCLEO-WL55JC2 demoboards.

I'm using the example code provided in the LocalNetwork_Concentrator and LocalNetwork_Sensor demos.

In the basic configuration, I cannot manage to have a communication distance range of more than 1m...

Do you know what the maximum ranges of these Nucleo boards?

Is there a setting to configure or is it a problem with the hardware design?

Thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Louis AUDOLY
ST Employee

Hello @joe_lambord​ ,

Which region have you configure via the AT command on the concentrator side ?

Regards