Posted on May 17, 2011 at 12:53Hi, Does ST provide USB audio driver for Window XP/Vista or Does ST use the standard protocols and no proprietary drivers are required? From the demo code downloaded from the website, I can find the drivers of mass st...
Posted on May 17, 2011 at 12:51Hi, STM1, So from RM0008, the I2S in the high-density devices can be configured as audio in /audio out, right? So we can use the I2S to input digital audio to the high-density devices and output to host via some trans...
Posted on May 17, 2011 at 12:51Most of the I2Ss configuration are supported for output functions only.We know that STM32F103xC support 2 I2Ss in it's design. Are the I2Ss birectional? Or any STM microcontroller supports birectional I2S interface? Th...