2008-11-24 2:20 AM
USB audio driver For STM32F103XX
2011-05-17 3:53 AM
Hi,
Does ST provide USB audio driver for Window XP/Vista or Does ST use the standard protocols and no proprietary drivers are required? From the demo code downloaded from the website, I can find the drivers of mass storage device and virtual com port. But the demo code for the audio speaker doesn't need audio driver in PC. If I want to output digital audio to PC via USB, do I need to implement the proprietary audio driver for it? Thanks. Best regards, Albert.. :)2011-05-17 3:53 AM
Dear Albert,
you do not need proprietary drivers to run Audio with STM32, the Provided Free USB kit uses Native Microsoft Drivers. Cheers, STone-32.