Hello!
I set my H563ZI I3C to master and attach it to another I3C secondary master. Now i want to test GETACCCR CCC. The firmware "en.stm32cubeh5-v1-2-0" only has the case that slave request mastership from current master. I want to know how to send ...
Hello! I dont know where to find received data after HAL_I3C_Ctrl_Receive_IT progress. I set I3C of my H563 as master and sent ENTDAA and master read , the slave answered both command. The interrupt of slave reflects that master re...
Hello! I have a H563ZI and a KEYSIGHT oscilloscope.I configured H563ZI as controller and sent an ENTDAA , then problem occired:
1.slave updated its dynamic address which as same as static address and different with what i set.
2.there ...
Hello ! Ijust found my h563zit6 has an 8-bytes rxfifo in i3c. I attach it to another i3c controller , and it olny received 8 bytes data. How can i receive data larger than 8 bytes? Thanks!
Hello Foued ! Thanks for reply! Sorry for my late reply. Finally i send GETACCCR successfully . I use the code from "STM32Cube_FW_H5_V1.1.0\Projects\NUCLEO-H563ZI\Examples\I3C\I3C_Controller_Switch_To_Target" .And if i want to use DDR transfer which ...