User Activity

I am looking to create a USB to I2S/TDM interface.I generated a Full Speed ​​USB AUDIO DEVICE skeleton from CUBE MX.I made some changes and I have working code in FS.I generated a skeleton in High Speed. I made the same changes and it doesn't work. T...
Hello, I want to use X CUBE USB AUDIO examples in X CUBE IDE.After generating the binary code (without errors) and flashing the binary code via DFU, the card is not recognized as an audio device, I tried on all 4 projects. I unplugged USB, do reset, ...
Hello,I want to try the examples in the package X CUBE USB AUDIO with X CUBE IDE and generate binary file for flashing it via DFU (I don't have ST LINK) .With others projects, I go to : project menu / properties / C/C++ build/ settings / MCU Post bui...
Kudos given to