As soon as possible...it's been 3 years now.Your TOOLS are useful so that people want to build with your PRODUCTS.Have you added these yet? It seems like it should be simple to change. I know if I were to have made this product, it would be simple ...
With the IS25LP128, are you setting the quad enable for the QSPI?When configuring it, you need to know that the QSPI is enabled (QE bit) and set the address, instruction, and data width appropriately. Depending on the instruction, you might have a 1...
Thanks. This part is interesting, as it is the same command for 1-bit and 4-bit modes. There is a 4-bit more QE configuration register which is set in the status register.
I'm working on this same chip right now for the U5 series using QSPI. I'd like to get it working correctly for just SPI first, since you have the special QE register bit that has to be properly set at initialization.Are you using your own initializa...