Hello @Anusree_k Can you try to use HSE bypass mode, in this mode you can provide an external clock signal directly to the HSE input pin (PA0). This mode only requires PA0, and PA1 can be used for other purposes.
Steps to Configure HSE in Bypass Mode...
Hello @BDoon.1 What you're observing is indeed a common behavior when using DMA in circular mode, especially when the DMA is first initialized and started.
When you first start the DMA transfer, the DMA controller may generate a transfer-complete (TC...
Hello @TBerg The issue you're encountering is likely due to the way the compiler optimizes and handles the complex expression in the first version of your code. When you break down the calculation into multiple steps, it becomes easier for the compil...
Hello @shivashankarr In order to reproduce the possible issue, could you please provide more details on your setting project if possible, attach your .ioc file/configuration?
Hello @PieroElectr At the beginning, can you please check I2S and DMA configurations:
Ensure that the DMA is configured to handle the I2S data stream:
Peripheral to Memory: YesData Width: 32-bit (to handle 24-bit data correctly)
Ensure that the I2S...