Hi @B.Montanari This is a great thread for a use case that I think is needed for many many deployment scenarios.Is the current state of the code example available somewhere on the ST site ?It would be great if this feature is an option to enable/conf...
I have the files under source control (Perforce/Helix, yes old school). Once I checked out stm32l4xx_hal_conf.h the 'Generate Code' seems to generate the appropriate updates. Should have better error checking/notification to not get into this state.
Thx,Now I have the MCU package downloaded, I configured the WWDG in the .ioc file and selected 'Generate Code'The main.c does not get updated and there are 'wwdg' related files in the STM32L4xx_HAL_Driver folder. There are some misc file in the main ...
Hi Rim,I have the same login issue. Our corporate network in blocking the myST login. At this time I just want to configure a WatchDog in the .ioc file. Does Cube really need to login to myST to do that ??If so what manual package do I download to be...